ATI and Güdel Announce New Coupling Technology for 3-Axis Press Transfer System
Apex, NC , julho 8, 2015
ATI Industrial Automation and Güdel, Inc. announce collaboration on transfer press systems where exchangeable transfer rails are secured by specially engineered ATI Tool Changers. This coupler upgrade mitigates common issues that cause other exchangeable rails to get stuck between die changes. With numerous production runs and die changes per day, this is a major productivity breakthrough for the customer.

It took collaboration between two industry leaders, ATI and Güdel, to solve one of the biggest problems with automatic die change for a world-class supplier: sticking “quick change” transfer rails. Now, with ATI and Güdel technology, the rails exchange in a smooth operation for continuous production and avoid millions of lost dollars in downtime. “Normally, one batch of parts runs while another is loaded for a die change,” said Joe Campbell, Vice President, Güdel. “If the rails fail to decouple properly, then the machine goes down. Now, with ATI Tool Changers, changeover is fast and reliable.” ATI is known for rigid, secure, and reliable coupling devices, such as industry-leading robotic tool changers.

ATI designed custom Tool Changers for Güdel transfer lines that can thoroughly withstand the high speed, high inertia loading environment that is typical with this process. "What was needed was an extremely strong coupling device that could handle the stress of the rail and die set during the exchange." said Robert Little, CEO, ATI. The simplicity of the Tool Changer design was also a clear benefit over the hydraulic system previously used which required lots of preventive maintenance, and caused downtime. ATI worked closely with Güdel to make sure they designed a Tool Changer with an appropriate locking mechanism, alignment pins, and sensors all contained in a package that met the required space constraints, while meeting all of the loading requirements. The press rail development with Güdel is just another example of ATI's willingness to work with the customer to make sure they create a custom solution that meets their needs.

ATI offers a wide selection of Tool Changer models to cover a variety of applications. Key features include: Excellent repeatability, high rigidity, and a lightweight and compact design. With over 25 years of robotic end-effector innovation, ATI’s engineering department, the largest of its kind for a robotic tooling company, is focused on developing cost-effective, state-of-the-art products and solutions. Güdel provides the ETR, or Electronic Transfer system, and the BDS (Blank De-stack System). All servo motions are linked with parallel operating encoders synchronized to the angle of the press. Fast and rugged, the system uses proven Güdel guideways with maintenance-free bearings and standardized parts. This eliminates service and maintenance costs for a more sustainable, cost-effective solution. “Güdel offers many ways to optimize cycle time for press lines, and we are proud to partner with world-class suppliers like ATI to solve difficult problems like this,” said Joe Campbell, Güdel Vice President.

More information on ATI Tool Changers here.

More information on Güdel here.

[Img1Link]
ATI Master- and Tool-Side Rail Tool Changer

[Img3Link]