ATI awarded U.S. Patent for Robotic Deburring Tool
Additional Patents Pending for the FlexdeburrTM
Apex, NC , janeiro 12, 2007
The United States Patent and Trademark Office has awarded ATI patent # 7,137,763 B2 for the Flexdeburr Robotic Deburring Tool. The patent applies to the air delivery method for the CNC version of deburring tool. The Flexdeburr CNC model is mounted in the tool holder of the customer's machining center and air is supplied axially through the machine's spindle. The patented Flexdeburr air supply system allows this air to be passed through the center of the joint allowing articulated motion of the deburring tool without the use of external hoses or fittings that might otherwise limit the free, compliant motion of the tool.

Since its release, the Radially-Complaint Deburring Tool has been recognized as a leader in the industry. This is the second patent that has been awarded to ATI for the Flexdeburr - additional patents are pending.

Complete information on the Flexdeburr is available on this website.

A new video demonstrating the Flexdeburr can be seen here.

[Img1Link]