New Products and Solutions at Automate 2024
Visit ATI at Booth 824
ATI will showcase a variety of live robotic demonstrations covering a diverse range of applications at the Automate show, May 6-9 at McCormick Place in Chicago, Illinois. Do not miss the opportunity to get an up-close look at all the latest ATI products and solutions, including:

A live grinding and sanding process will showcase the CGV-900 Compliant Angle Grinder and AOV-10 Robotic Orbital Sander. A FANUC M-10iD/16 robot will be using ATI QC-29 Robotic Tool Changers with an attached large air port module, to switch between the grinding and sanding tools.

ATI will also demonstrate how their Axia80 Force/Torque (F/T) Sensor and a KUKA KR6 Robot can perform a planetary helical gear meshing operation using force control.

Staubli Robotics will demonstrate how ATI's Force/Torque Sensors and a Staubli cobot can be utilized in robotic surgery through force-controlled robotic hand-guiding.

In a large cell, ATI will also demonstrate how their Heavy Automation Tool Changers are used to automatically switch large end-effectors. A FANUC R-1000iA/80F robot, utilizing ATI QC-210 Tool Changers, will simulate the joining of automotive B-pillar assemblies by tool changing between an Atlas Copco K-Flow flow drill fastening tool and an Atlas Copco SCA industrial dispensing tool.

Additionally, ATI will display the new MC-50 Manual Tool Changer. With intuitive and ergonomic lever operation, the patent-pending MC-50 provides a simple solution for quickly changing robotic end-of-arm tooling by hand. This compact and robust Tool Changer is designed for applications on collaborative robots that support payloads up to 25 kg and small industrial robots supporting payloads up to 10 kg.

To learn more about how ATI's innovative end-effector products and solutions can help increase robotic flexibility in your application come talk to our knowledgeable team in Booth 824 at Automate!

Contact us for more information on any of our products.

Click here for Automate show information and registration.

[Img1Link]
See ATI's New MC-50 Manual Tool Changer in Action!