ATI Develops New Series of Manual Tool Changers
Unique Design Combines High Strength and Excellent Repeatability
Apex, NC , junho 24, 2010
ATI Industrial Automation has developed a new series of Manual Tool Changers that provides a cost-effective solution for quickly changing tools by hand. They feature a unique design that combines high strength, excellent repeatability and a patent-pending screw-cam locking mechanism with multiple fail-safe features, which resists vibration and prevents loosening. The new Manual Tool Changers also feature quick-action locking for one-handed manual operation. These robust and compact Manual Tool Changers can handle payloads up to 80 pounds (36 kg) and pass pneumatics and electrical signals.

ATI will introduce two new Manual Tool Changer models, the MC-16 and the MC-36, at the 2010 IMTS show on September 13-18, in Chicago, IL, booth # N-6429 and at the 2010 ATE show on September 28-30, in Rosemont, IL, booth # 721. ATI will also have all of their newest end-effector products on display, including Robotic Tool Changers, Multi-axis Force/Torque Sensors, Robotic Deburring and Finishing Tools, Robotic Collision Sensors, Rotary Joints, and Compliance Devices. If you would like a free pass to the show, contact ATI at info@ati-ia.com or +1 919-772-0115.

More information on the 2010 IMTS show here.

More information on the 2010 ATE show here.

More information on our Manual Tool Changers here.

[Img1Link]
MC-36 Master and Tool-side Manual Tool Changer