New Tool Changer Modules for Aluminum Welding

High Current and High Flow

Apex, NC,  agosto 4, 2013
 

Spot welding aluminum is a resistance welding method used to join two or more overlapping metal sheets. Typically, two copper electrodes clamp the metal sheets together and current is passed through the material. The resultant heat generated by electrical resistance creates a pool of molten material between the copper electrode tips. When the current is stopped, the copper tips cool the spot weld, causing the metal to solidify under pressure.

The water-cooled copper electrodes are essential to remove the surface heat quickly, accelerating the solidification of the metal. ATI’s new Tool Changer Utility Modules have been specifically engineered to accommodate these high coolant flow requirements. ATI’s FF4 module is a fluid/air module supporting five ½ inch hoses. With two feed lines and three return lines, the FF4 module can pass enough cooling water for nearly any robot-carried weld gun, allowing the weld gun to cool the electrode correctly and maintain consistent weld quality.

ATI’s new Tool Changer Utility Modules have been designed to allow for large power cable diameter and are able to handle continuous high current transfer without failure. ATI’s PH3 module is a primary current module that supports 0000 AWG or 100 mm2 cables. This is much larger than the 2 AWG or 35 mm2 cables typically used for welding steel. ATI also offers Tool Changer Utility Modules to support clinching, riveting, bolting, flow drill screws, and other joining methods commonly used for aluminum.

ATI offers a wide selection of Tool Changer models and Utility Modules to cover a variety of applications. Key features include: Excellent repeatability, high rigidity, and a lightweight and compact design. With over 20 years of robotic end-effector innovation experience, ATI’s engineering department, the largest of its kind for a robotic tooling company, is focused on developing cost-effective, state-of-the-art products and solutions.

More information on our FF4 Fluid/Air Utility Module here.

More information on our PH3 Fluid/Air Utility Module here.

More information on our Robotic Tool Changers here.

 



More Featured Stories
 
HyperLink View our October 2024 eNewsletter!
(out 2024)

HyperLink Cutting-Edge Solutions at FABTECH 2024
(set 2024) Visit ATI at Booth W5281

HyperLink ATI Develops the MC-50 Manual Tool Changer
(set 2024) Unmatched performance, reliability, and quality for manual exchange of robotic tooling

HyperLink View our September 2024 eNewsletter!
(set 2024)

HyperLink ATI Force/Torque Sensors for Surgical Robotics
(ago 2024) Assisting Surgeons with a Robotic Sense of Touch