FLEXIBLE ROBOTIC DEBURRING FROM ROBODK, DIY AND ATI
ATI Industrial Automation, DIY-Robotics and RoboDK combine their complimentary expertise in a user-friendly solution for a variety of material removal applications. Utilizing a ‘plug and play’ approach, the three companies have designed the Robotic Deburring Cell to perform a plethora of light-duty material removal operations. The Robotic Deburring Cell allows users to get their material removal process up and running quickly, with confidence, and gives them the flexibility and control to evolve their process over time.
Read More >
[hlNewsImg]


ROBOTIC WELD BEAD REMOVAL WITH ATI’S FORCE/TORQUE SENSORS
Sponsored by the Advanced Robotics for Manufacturing Institute (ARM), a group of engineers at The Robotics Institute of Carnegie Mellon discovered a way to tackle two of these challenging material removal operations in one solution. With support from research and development experts from Siemens Technology as well as application guidance from Yaskawa, these automation experts devised a breakthrough system that uses robots to remove weld beads from inside a tube.
Read More >
[hlNewsImg]


ATI MATERIAL REMOVAL IS CRX-READY
ATI continues to expand cobot offerings and is pleased to announce that FANUC CRX users can now integrate a variety of automated material removal operations like chamfering, edge-deburring and finishing, removal of flash and parting lines, sanding, and more with ATI’s Material Removal Tools. Designed for simplicity, each all-in-one CRX-Ready Kit includes the end-effector along with anything else needed to get the CRX application connected and running.
Read More >
[hlNewsImg]


ATI UTILITY COUPLERS HELP KTH ELIMINATE EQUIPMENT FAILURES
There is no better way to resolve a problem than eliminating it entirely. At KTH Parts Industries Inc., automating a manual equipment changeover process using ATI’s Utility Couplers accomplished that very feat. To increase flexibility and optimize limited manufacturing floor space, KTH created a dual-sided work cell with a turntable. The new process eliminates roughly 65 hours per year of downtime per line, reduces the total cost of operations, and increases equipment utilization and productivity.
Read More >
[hlNewsImg]


ATI DEVELOPS SPACE-RATED F/T FOR MARS 2020 ROVER
After launching in July of 2020, Perseverance Rover finally landed on Mars in February of 2021. Since then, Perseverance has been hard at work, exploring, investigating and discovering the planet's surface and sending updates along the way. The journey to Mars actually began for ATI many years ago when the company underwent an epic project to develop Force/Torque Sensor technology that would not only survive, but thrive on the red planet.
Read More >
[hlNewsImg]


ATI JOINS NOVANTA!
ATI has officially joined Novanta, Inc! Novanta is a leader in mission critical technologies such as drives, motors, encoders, and precise motion to medical and advanced industrial equipment manufacturers. ATI develops robotic end-effectors with a focus on tool changing, material removal and force/torque sensing. The combination of these two companies will strengthen all their product offerings for the most demanding robotic and automation applications.
Read More >
[hlNewsImg]


Featured Products

[hlImage]

ATI DEVELOPS ULTRA-THIN FORCE/TORQUE SENSOR
ATI’s Mini43LP can enhance the accuracy and repeatability of research and development, product validation, assembly, and other micro force sensing applications. It is the ideal force sensing option for small delicate operations such as the assembly of electronic components or optics, product research and testing applications, laboratory automation, robotic surgery, and more.
Read More >
[hlImage]

UNLOCK PRODUCTIVITY WITH THE QC-29 ROBOTIC TOOL CHANGER
The QC-29 Robotic Tool Changer brings the powerful and rugged technology of ATI’s Heavy Duty Tool Changers to the 25-35kg payload class. The QC-29 is the first standard ATI Tool Changer designed with a rectangular body that mounts directly to 40mm and 50mm robot wrists.
Read More >
Featured Videos

[hlImage]

LET'S TALK CV14 CONTROL MODULE
ATI’s CV14 Control Module makes a great addition to many tool changing applications. By including built-in features like lock/unlock sensors, an integrated valve, I/O and tool identification, this versatile and robust control module allows users to optimize their process without increasing footprint or implementation time.
View >
[hlImage]

WHY ATI MATERIAL REMOVAL?
Our knowledge of robotic systems and applications extends far beyond end-of-arm tools. We want to help you choose the right product, and our hope is to partner with you to bring your ideal solution to reality. In addition to material removal equipment, ATI customers have access to product testing, application experts, and partner integrators to further support their automation journey.
View >


Upcoming Events

ATI exhibits at a variety of industry shows and conferences. Our schedule is listed below. Contact Valerie Van Deusen here if you would like a ticket or pass (subject to availability) to any upcoming shows.